Australia | english

17Apr.,2014

PNOZmulti 2 with Powerlink connection

The new POWERLINK communication module is now available for the configurable control system PNOZmulti 2.

The new POWERLINK communication module enables the PNOZmulti 2 base unit to be expanded on the left-hand side and to be connected to a Powerlink network. As such there is now another communication module available alongside Profibus-DP, EtherCAT, CANopen and Modbus TCP.

Powerlink combines the benefits of Ethernet and fieldbus in one system: the original Ethernet properties with proven, robust CANopen mechanisms, plus real-time capability.


Your benefits at a glance:

  • Option to connect to Powerlink networks (supports CANopen
    over Ethernet)
  • Real-time communication with a higher level Powerlink
    master control system
  • Two-way signalling and control via the communication module
  • Diagnostic concept PVIS can be activated in the PNOZmulti Configurator,
    individual customer texts can also be integrated


Play it safe and use PNOZmulti 2 – the worldwide safety standard for all machine types.


Further information:

Configurable control system PNOZmulti 2

The PNOZmulti 2 is now available with POWERLINK connection