Australia | english

21May,2015

Reduced engineering – shorter project run times

With the automation system PSS 4000 you can reduce your engineering.

On many automation systems, the hardware must be selected to carry out the configuration or programming. Subsequent modifications are very costly.


On the automation system PSS 4000, it's different: the hardware can be selected and the program allocated to the hardware at a much later point in the process, as it is largely independent of the configuration stage.


This provides many advantages:

  • Shorter project run times as subtasks are processed in parallel: hardware can be selected and the program allocated to the hardware at a much later point in the process
     
  • Machine can be expanded retrospectively: the user program can be distributed to another control system without any great effort
     
  • Partial commissioning and partial operation of individual machine parts: so you can be flexible and independent when creating your application and during operation


Further information:

Automation system PSS 4000

With the automation system PSS 4000 you can reduce your engineering.