Australia | english

Press releases

Category
With the Pilz System Partner Programme, from challenges to solutions: System partners are Pilz-certified companies that offer complete solutions with Pilz product and systems.

Ostfildern, 2Jul.,2019

Global professional network for safe automation - Pilz System Partner Programme – worldwide

With a System Partner Programme, the automation company Pilz is increasing the presence of its products and solutions worldwide: In future, customers will also be able to obtain complete safe automation technology solutions from Pilz via selected, certified partners.

Press message
The world's first safe radar system solution expands the safe sensor technology range PSEN from Pilz.

Ostfildern, 23May,2019

World's first safe radar system solution new to the Pilz portfolio - Safe even in the most rugged environments!

New to the Pilz portfolio is the world's first safe complete solution for protection zone monitoring, based on radar technology. It comprises the safe radar system "LBK System" from Inxpect S.p.A. and the configurable small controller PNOZmulti 2. This complete solution provides safe, economical monitoring even in the must rugged environments – in extreme production environments such as dust in woodworking for example – or with complex plant structures. Benefits of the safe radar system solution include high plant or machine productivity, despite the most rugged environment.

Press message
Pilz is a solution supplier for automation: in the field of service robotics, for example, the company is developing software to control robots.

Ostfildern, 23May,2019

Moderate increase in turnover and rise in employee numbers for Pilz in 2018 - "Growth in a difficult environment"

The Pilz group of companies remains on course for growth, despite the economic downturn: in the last financial year, 2018, the automation company had a turnover of 345 million Euro (+2.1 %). The number of employees rose above 2,500 for the first time.

Press message
The safe voltage monitor PNOZ s60 monitors the de-energised state of plant and machinery to UL 6420.

Ostfildern, 1Apr.,2019

Keeping it de-energised

With the safe voltage monitor PNOZ s60 Pilz now offers monitoring of the de-energised state of plant and machinery to the standard UL 6420. This makes PNOZ s60 suitable for use in applications that require a Safety Lockout System (SLS), that is, when plants are held in a safe, electrically de-energised state.

Press message
Pilz offers a services package for compliance of machinery on the US market.

Ostfildern, 19Mar.,2019

Machinery safety: Pilz is expanding its international range of services - have a nice trip! US compliance for machinery

Pilz is expanding its international range of services in the field of machinery safety: in future Pilz will support companies worldwide who want to export machines to the USA or operate them there, in terms of the necessary compliance. Manufacturers and operators can ensure that their plant and machinery complies with the US requirements for machinery safety.

Press message
The “Security” white paper from Pilz helps to understand central aspects of security and to put solution approaches into practice.

Ostfildern, 13Mar.,2019

“Security” at a glance: New white paper from Pilz

New strategies for the safety of plants and machines must take into account both security (IT security) and also safety (machinery safety). Pilz shows how this is possible in the “Security” white paper.

Press message
The safety laser scanners PSENscan from Pilz now provide flexible monitoring of vertical areas.

Ostfildern, 26Feb.,2019

Safe use also in the vertical position!

The safety laser scanners PSENscan from Pilz are now also suitable for area guarding of vertical applications, for example for access protection. What’s more, with PSENscan applications can now be designed with greater flexibility, which minimises downtimes and increases cost-effectiveness.

Press message
With the new IO-Link master module PSS u2 ES 4IOL the remote I/O system PSSuniversal 2 can now communicate with sensors and actuators via the globally standardised IO interface.

Ostfildern, 19Feb.,2019

IO-Link technology for PSSuniversal 2 - The link to networked production

Pilz is presenting the new IO-Link master module PSS u2 ES 4IOL for communication between the remote I/O system PSSuniversal 2 and sensors/actuators. IO-Link technology is standardised worldwide in accordance with IEC 61131-9. It enables automatic parameterisation and expanded device diagnostics in the spirit of Industrie 4.0.

Press message
The modular operating mode selection and access permission system PITmode combines safety and security in one system.

Ostfildern, 14Feb.,2019

Access permission plus operation mode selection now modular - fusion of safety and security

With PITmode fusion, Pilz now offers a modular operating mode selection and access permission system. The modular system is characterised by more flexibility for functionally safe operating mode selection and for the control of access permissions to plant and machinery. This way, PITmode fusion enables efficient operation mode selection and access permission management that covers both safety and security specifications.

Press message
Robust communication: Two new control heads with M12 interfaces supplement the railway range of the automation system PSS 4000-R from Pilz.

Ostfildern, 11Feb.,2019

M12 interfaces for safe signal transfer

In the automation system PSS 4000-R for railway, Pilz now provides two new control heads with M12 interface. So reliable signal transmission is guaranteed on and beside the track, even under adverse conditions!

Press message
Under the motto “We automate. Safely.” in 2019 Pilz will again be presenting innovative automation solutions for all industries at the Hannover Messe.

Ostfildern, 5Feb.,2019

Pilz at the Hannover Messe 2019, Hall 9, Stand D17 - Automation in the “Spirit of Safety”

Under the motto “We automate. Safely.” in 2019 Pilz will again be presenting innovative automation solutions for all industries at the Hannover Messe from 1 to 5 April. The pioneer of safe automation will be focusing on innovations from the areas of operating and monitoring, safe sensor technology, I/O systems and services. Accompanied by: The world’s lowest profile actuator and a modular, therefore innovative operating mode selection and access permission system.

Press message
With training for the

Ostfildern, 15Jan.,2019

New qualification as "CECE – Certified Expert in CE Marking" - CE marking at the highest level

Pilz expands its international training offer with a further TÜV certification: The new training for "CECE – Certified Expert in CE Marking" provides expert knowledge about all necessary steps on the path to CE marking.

Press message
Thanks to increased performance, the new generation of Pilz Motion Control systems PMCprimo C2 offers higher cycle counts and therefore new production quality.

Ostfildern, 18Dec.,2018

Pilz launches new generations of the control systems PMCprimo C2 from the Pilz Motion Control range - More power!

Thanks to increased performance, the new generation of Pilz Motion Control systems PMCprimo C2 offers higher cycle counts and therefore new production quality. A wide number of interfaces and an encoder input, digital inputs/outputs and a USB interface for data import and export ensure a high level of flexibility.

Press message
For the configurable safe small control system PNOZmulti from Pilz, a new application simulation is available from Version 10.9. Users can test the configured user program even before commissioning, and thereby save time and costs during configuration.

Ostfildern, 26Nov.,2018

Configurable safe small control system PNOZmulti from Pilz new with application simulation - simulate the configuration now also offline!

From Version 10.9 of the Software tool PNOZmulti Configurator, PNOZmulti projects of the configurable safe small control systems can be simulated offline, completely without the use of hardware. That way, Pilz provides a user-friendly aid to detect, analyse and remedy errors at an early stage.

Press message
Learning in practice and understanding better: With Pilz Education Systems, Pilz offers a modular training system for the range of safe automation technology.

Ostfildern, 31Oct.,2018

Modular training systems Education Systems PES - Safe automation: Learning how to do it

With the Pilz Education Systems (PES) Pilz launches a modular training system on the market. With this, the institutions of training/further education can improve the practical training in the field of safe automation technology.

Press message
In addition to finger and hand protection, the light curtains PSENopt II are available from now also as versions with body protection. With a shock resistance of 50 g, PSENopt II are extremely robust with regard to shocks, vibrations and collisions.

Ostfildern, 30Oct.,2018

New version light curtains PSENopt II with body protection - Safety from tip to toe

Pilz completes its light curtain portfolio: In addition to finger and hand protection, the light curtains PSENopt II are available from now also as versions with body protection. Thanks to high robustness, fast diagnostics and comprehensive accessories, access to hazardous areas can be safeguarded economically.

Press message
Lifetime achievement award: As part of the 10. Mechanical Engineering Summit, Renate Pilz received the

Ostfildern, 24Oct.,2018

"Preis deutscher Maschinenbau" (Award of German Mechanical Engineering) awarded to Renate Pilz - Businesswoman awarded for her life's work

For her life's work, businesswoman Renate Pilz receives the "Preis deutscher Maschinenbau" (Award of German Mechanical Engineering) 2018. She received the award on Tuesday, 16. October at the 10. Mechanical Engineering Summit. According to the expert jury, the consequent value-based corporate culture of Pilz GmbH & Co. KG. is to be particularly honoured. Renate Pilz is the first woman to receive this award.

Press message
The main focus of the Pilz stand at the SPS IPC Drives 2018 will be on safe sensor technology.

Ostfildern, 9Oct.,2018

SPS IPC Drives 2018: Pilz brings to life safe sensor technology - automate with all your senses

At this year's SPS IPC Drives in Nürnberg (27. - 29.11.2018) Pilz will focus on safe sensor technology: The automation company shows components and complete solutions for the most varied applications of sensor technology in action. It is a premiere in Nürnberg for the new light curtains PSENopt II for body protection. Innovations in drive technology Pilz Motion Control (PMC) and the new qualification as a "CECE – Certified Expert in CE Marking" are also part of the exhibition presence.

Press message
The new energy stores PMCenergy SD save energy, used in conjunction with the servo amplifiers PMCprotego D and PMCtendo DD5! In the process, the existing brake energy is absorbed, buffered and provided again, without mains feedback.

Ostfildern, 2Oct.,2018

New energy store PMCenergy SD uses braking energy - If you brake, you economise!

Pilz expands its range of energy-efficient drive technology: The new energy stores PMCenergy SD save up to 60 % of energy when used in conjunction with the servo amplifiers PMCprotego D and PMCtendo DD5. For this, the braking energy created in a braking process is absorbed, buffered and provided again - without mains feedback.

Press message
The non-contact, magnetic safety switch PSENmag in the stainless steel variant enables safe gate and position monitoring under harsh conditions.

Ostfildern, 6Aug.,2018

Despite dirt and temperatures! - Magnetic safety switch PSENmag from Pilz now also as a stainless steel variant

The magnetic safety switch PSENmag in the stainless steel variant reliably monitors safety gates and positions in harsh industrial environments up to 120 °C and instils confidence with its long service life.

Press message

Ostfildern, 1Aug.,2018

Ready for the digital age of rail – InnoTrans 2018: Pilz presents comprehensive Industrie 4.0 solutions for the rail industry

At InnoTrans 2018, from 18-21 September 2018, automation systems provider Pilz will present its comprehensive solution offerings for digitalisation on trains and railway lines. Beyond control system solutions with the PSS 4000-R automation system, Pilz offers complete solutions up to and including completely pre-wired control cabinets. On September 21, as part of the InnoTrans Convention, Pilz will present ideas in the “Innovative paths 4.0 – VDB future workshop” on the topic of “Industrie 4.0 – Rail 4.0: Opportunities for mid-sized companies”.

Press message
The analogue input module PNOZ m EF 4AI expands the product range of configurable small control systems PNOZmulti 2 from Pilz and it offers faster processing and optimised diagnostics.

Ostfildern, 12Jul.,2018

New analogue input module for configurable safe small control system PNOZmulti 2 from Pilz optimises processes - temperature, fill level etc. recorded safely

The new analogue input module PNOZ m EF 4AI expands the product range of configurable, safe small control systems PNOZmulti 2. It can be used to safely record and monitor any process up to PL e or SIL CL 3. One particular advantage is the separate module program (mIQ) with can be used to make fine-granular adjustments of the value. This ensures faster processing directly in the module, process monitoring is not only safer, but also more exact.

Press message
The fifth edition of the Safety Compendium has now been published, providing an orientation for functional safety.

Ostfildern, 28Jun.,2018

Pilz provides an orientation for machinery safety

Validation of robot applications to ISO/TS 15066, safe programming to EN ISO 13849 or risk evaluation and analysis to IEC 62061. Anyone who deals with functional safety can easily get entangled in the standards and directives. With its Safety Compendium Pilz is giving design engineers, manufacturers and operators a reliable orientation for the most important machinery safety directives. The 5th version of this standard reference work has now been published.

Press message
Human-robot collaboration in axle drive assembly, BMW Group Dingolfing plant: BMW Group is working together with Pilz on safety. Image: BMW Group

Ostfildern, 18Jun.,2018

CE marking for robot assistance systems of the BMW Group - Pilz protects HRC applications in car production

For safety when working with robot assistants, the BMW Group works together with Pilz: the automation company carries out the conformity assessment including final CE marking. That enables Pilz to ensure safe human-robot collaboration (HRC) at multiple production sites of the BMW Group.

Press message
The new dual-pole semiconductor output module PNOZ m EF 8DI2DOT of the configurable safe small control systems PNOZmulti 2 ensures the safety of a complete press.

Ostfildern, 29May,2018

More efficiency and higher safety at presses! - Pilz expands the configurable safe small control systems PNOZmulti 2 by dual-pole semiconductor output modules PNOZ m EF 8DI2DOT

Safe monitoring of mechanical presses is guaranteed by the new dual-pole semiconductor output module PNOZ m EF 8DI2DOT of the configurable safe small control systems PNOZmulti 2 from Pilz. This means that press safety valves and other actuators that require dual-pole switching can be controlled simply and flexibly. This enables not only safer, but also clearly more productive management of the operation of mechanical presses.

Press message
The area Motion Control at Pilz – PMC – has been expanded by the operator terminal PMI 6 primo with PLC, Motion and CNC functionality.

Ostfildern, 15May,2018

Pilz expands its product range in the Motion Control area by a new operator terminal PMI 6 primo with control, motion and CNC function - control and visualisation of "primo" drives!

Now the solution package Pilz Motion Control (PMC) includes the operator terminals PMI 6 primo, with their PLC, Motion and CNC functionalities. Within the plant, they perform not only automation including motion management, but also the visualisation or project planning. This equipment enables the user to have a more flexible application, if required.

Press message
At this year's Automatica, the automation business Pilz also introduces its modules for service robotics for the first time.

Ostfildern, 14May,2018

Automatica 2018: Premiere for Pilz service robotics modules - service robotics goes Industry

On the Automatica from 19. To 22. June, the automation company Pilz shows its system solutions for the service robotics range: It is a premiere in Munich for the new service robotics modules of the company. Further exhibition topics are the comprehensive Pilz service portfolio and the offer of safe sensor technology for robot cells and for human-robot-collaboration (HRC). The visitors will also receive an insight into the R&D activities of the automation company.

Press message
Pilz SecurityBridge is used within a corporate network and prevents unauthorised access to controllers.

Ostfildern, 20Apr.,2018

Pilz SecurityBridge protects controllers from manipulation and unauthorised access - On the safe side with SecurityBridge

If people, machinery and industrial processes are intelligently linked, these networks are also more susceptible to attack. The Pilz SecurityBridge protects the configurable, safe small controllers PNOZmulti and the automation system PSS 4000 from network-based attacks and unauthorised access. Plant and machinery are thus not only safe, but also secure, which ensures the safety of employees and increases the availability of the machinery.

Press message
The automation company Pilz wants to continue growing with a complete offer for safe robotics: In 2018, the company provides the modules for service robotics on the market, including a self-developed robot arm.

Ostfildern, 12Apr.,2018

Pilz continues to grow in turnover and number of employees- new to the portfolio: Modules for service robotics: "Grateful for a successful year 2017."

The Pilz GmbH & Co. KG Group continues to grow: In the last financial year 2017 the automation company increases its turnover to 338 Mio Euro and the number of employees to about 2.300. The demand on the Asian market has grown particularly strongly. In 2018, the family business wants to continue growing and it also promotes a new, modular offer for service robotics.

Press message
With the Pilz Service Robotics modules, Pilz offers a set for service robot applications in an industrial environment.

Ostfildern, 12Apr.,2018

Pilz expands its portfolio by modules for service robotics in an industrial environment - Pilz service robotics modules - open for service tasks in industry

The automation company Pilz expands its portfolio by the new product range Service Robotics: The Pilz Service Robotics modules include initially the robot arm, the control module and the operator module. The essential features are openness, i.e. thanks to the software framework ROS, user-friendly operation and fast commissioning according to the plug-and-play principle. This enables users to assemble their individual service robot applications.

Press message
The range of safety gate systems PSENmlock for safe interlock and safe guard locking now offers a new version for series connection.

Ostfildern, 9Apr.,2018

New products and versions for the modular safety gate system from Pilz – safety gate sensor PSENmlock with series connection, pushbutton unit PITgatebox and escape release – systematic protection for every gate!

The modular safety gate system from Pilz offers individual safety gate solutions that are ideally tailored to the requirements of the most varied applications. Users benefit from an economical series connection, rapid diagnostics, additional control and pushbutton elements and an optional escape release. Different components can be combined to fit the application. So users achieve an individual safety gate solution, ideally tailored to the respective application. The safety gate system now includes the safety gate sensors PSENmlock with series connection and the pushbutton unit PITgatebox.

Press message
Modular to the factory of the future: On the Hannover Messe, Pilz shows innovative automation solutions for safety gate monitoring, among them safety gate systems and sensors.

Ostfildern, 6Mar.,2018

Pilz at the Hannover Messe 2018, Hall 9, Stand D17 - Modular to the factory of the future:

Under the motto "We automate. Safely." Pilz will be presenting innovative automation solutions for the factory of the future at the Hannover Messe from 23 to 27 April 2018. In the focus of this year's presence at the exhibition there is the topic of "modular safety gate system". In this context, Pilz presents its new version of the Industry 4.0-compatible safety gate system PSENmlock. Furthermore, the automation expert presents novelties from the range of safety and control technology. The Safe human robot collaboration is also in the focus of this year's presence of Pilz.

Press message
CMSE® - Certified Machinery Safety Expert is a globally recognised qualification enabling a 360° approach to machinery safety. CMSEs can pursue recertification to advance their knowledge base and remain up to date.

Ostfildern, 2Feb.,2018

Recertification of CMSE® - Certified Machinery Safety Expert qualification - Updating knowledge, assuring continuing expertise

Pilz and TÜV Nord have been setting an international standard for machine safety qualification since 2013 with their CMSE® - Certified Machinery Safety Expert programme. CMSEs can pursue recertification to advance their knowledge base, remain up to date with the latest developments in the field of machine safety and retain their certification.

Press message
The remote I/O system PSSuniversal 2 has been expanded by a head module with an EtherNet/IP interface. So the open system adapts perfectly to the system environments that already exist.

Ostfildern, 21Dec.,2017

New head modules for EtherNet/IP: Pilz expands remote I/O system PSSuniversal 2 - For more openness in the periphery

Pilz expands its remote I/O system PSSuniversal 2 by a head module with EtherNet/IP interface. This means that PSSuniversal 2 offers the necessary openness for smooth communication in various control environments on an Ethernet basis.

Press message
The camera-based protection system PSENvip 2 provides a new version for special purpose presses: PSENvip Long Range is ideal for press brakes with monitoring of up to 18 meters.

Ostfildern, 4Dec.,2017

PSENvip Long Range - safety at full length!

The camera-based protection system PSENvip 2 for press brakes from Pilz provides a new Long Range version: PSENvip Long Range is the first protective device with a protection range of up to 18 meters. That makes the robust protection system ideal for monitoring special presses such as tandem presses. The camera-based protection system fulfils all common safety standards and also EN 12622, so that PSENvip 2 guarantees maximum productivity with simple handling.

Press message
PSS67 PLC from Pilz is the first safe PLC controller with protection type IP67. It is particularly suitable for automation tasks in distributed plants.

Ostfildern, 23Nov.,2017

PSS67 PLC: The world's first PLC controller for safety and automation with protection type IP67 - Automation outside the control cabinet

With PSS67 PLC, the automation company Pilz is launching the first safe PLC controller with protection type IP67. PSS67 PLC can be installed outside the control cabinet, directly on the machine. This means that users can save space, reduce their wiring work and enjoy greater flexibility when implementing decentralised control architectures.

Press message
For the Motion Monitoring modules PNOZ m EF 1MM and 2MM of the configurable small controller PNOZmulti 2 two new functions are available for drive monitoring.

Ostfildern, 13Nov.,2017

Configurable, safe small controllers PNOZmulti 2 with new Motion Monitoring functions - SLA-M and SAR-M for drives

For the Motion Monitoring modules PNOZ m EF 1MM and 2MM of the configurable small controller PNOZmulti 2, two new safety functions are now available for drive monitoring: For safely limited acceleration SLA-M and the safe acceleration range SAR-M. The new motion monitoring functions are available from software version 10.6 of PNOZmulti Configurator. They ensure additional safety and productivity at plants and machines.

Press message
The configurable small controllers PNOZmulti 2 now have the expansion module PNOZ m EF SafetyNET for the safe communication of data via SafetyNET p.

Ostfildern, 2Nov.,2017

Configurable safe small controllers PNOZmulti 2 now with communication via SafetyNET p - Safely connected in the system

The configurable small controllers PNOZmulti 2 from Pilz allow the linking of SafetyNET p via the safe real-time Ethernet, effective immediately. Up to 16 base units can be linked via the expansion modules PNOZ m EF SafetyNET. A safe connection and data transfer between the small controllers is thereby possible. The network configuration is performed with the software tool PNOZmulti Network Editor. The configuration of projects is thus made easy. In addition, PNOZmulti and PNOZmulti Mini systems can also be incorporated into the network using multi-link modules.

Press message
The pressure-sensitive safety mat PSENmat from Pilz combines safe area monitoring with machine operation.

Ostfildern, 27Oct.,2017

The pressure-sensitive safety mat PSENmat from Pilz combines safe area monitoring with plant and machine operation - “virtual” control

With PSENmat, the automation company Pilz is now introducing its own pressure-sensitive safety mat, developed in-house: A world first is the integrated position detection that provides the operator with a control function – similar to a virtual button. PSENmat thereby combines safe area monitoring with plant and machine operation in one sensor. It enables totally new machine control concepts.

Press message
With its smart factory model, at SPS IPC Drives 2017 Pilz will be exhibiting not only product innovations but also Industrie 4.0 you can touch.

Ostfildern, 6Oct.,2017

Pilz will be showing world firsts at SPS IPC Drives 2017 - Automation: Safety for every dimension

At SPS IPC Drives 2017 in Nuremberg (28.-30.11.) Pilz will be showing how human and machine can work together more closely and therefore more productively and ergonomically thanks to dynamic safety solutions. Among the world firsts are the controller PSS67 PLC, the first safe PLC controller with IP67 protection and the pressure-sensitive safety mat PSENmat with position detection.

Press message
Pilz provides support from risk assessment to safety validation, to guarantee that machines comply with the requirements of NR-12 in Brazil.

Ostfildern, 7Sep.,2017

Pilz provides support with international compliance: the safe route to NR-12-compliant machinery for Brazil - Machinery safety: Passport to Rio

Pilz is expanding its range of services for international compliance: the automation company can now also support its customers en route to NR-12-compliant machinery, thus opening up access to the Brazilian market to machine builders and users all over the world. That's because: any manufacturer who sells machinery to Brazil must supply this machinery in compliance with the Brazilian regulatory standard (Norma Regulamentadora) NR-12. In turn, operators of machinery in Brazil are obliged to put in place protective measures for their employees in accordance with NR-12.

Press message
Tooled up for starting their career: on their first day, the new apprentices and dual students at Pilz were given not only important information by their trainers, but also their own personal toolbox.

Ostfildern, 4Sep.,2017

New training year at Pilz in Ostfildern: one third female apprentices and additional dual study courses - focused on promoting skills

The new training year at the automation company Pilz in Ostfildern started on 4 September. A total of six apprentices and six students from the Baden-Württemberg Cooperative State University (DHBW) embarked on their professional career. One of the apprentices and three of the new students are female. From 2018 the company will have more dual courses as well as a new apprentice place in addition to those already offered in the training programme.

Press message
Christian Erles is the new Vice President of Sales International at the automation company Pilz.

Ostfildern, 22Aug.,2017

Christian Erles, new Vice President of Sales International at Pilz - Newly established Sales with a new Head

Global and international: The automation company Pilz from Ostfildern has completed the reorganisation of its international Sales department. As the new Vice President of Sales International, Christian Erles works at the forefront of international Sales activities.

Press message
Small controllers PNOZmulti can now be linked directly to the visualisation software PASvisu. As a result, the full function range of the software is available, including the diagnostic option.

Ostfildern, 10Jul.,2017

New version of the web-based visualisation solution PASvisu - Optimum combination of controller and visualisation

Pilz is extending its web-based visualisation solution PASvisu: There is a new alarm management function, plus an OPC UA interface for connection to small controllers. For users of the configurable small controllers PNOZmulti, PASvisu now also allows a direct connection. As a result, the visualisation includes the full function range of the controller software, including the diagnostic option.

Press message
Pilz Award 2016 recognises the achievements of suppliers: Each year since 2006, Pilz GmbH & Co. KG has honoured its five top suppliers.

Ostfildern, 6Jun.,2017

Pilz Award 2016 for the top suppliers - Thomas Pilz: Values are the basis of good business relationships

The automation company Pilz from Ostfildern near Stuttgart has presented its five top suppliers with the Pilz Award 2016. The awards were presented by Thomas Pilz, Managing Partner of Pilz, during an official ceremony. The family business uses the Pilz Award to recognise outstanding quality, high delivery reliability and partnership-based cooperation.

Press message
The new force and pressure measurement system PROBms from Pilz is used to demonstrate that the safety requirements comply with the applicable standards for HRC, in this case in accordance with ISO/TS 15066.

Ostfildern, 10Apr.,2017

New force and pressure measurement system PROBms guarantees the standard-compliant safety of human robot collaboration (HRC) - Safe rental for HRC!

With the new rental-based force and pressure measurement system PROBms Pilz now offers a complete package for validation of human-robot collaborations (HRC) in accordance with ISO/TS 15066. So the limit values for force or pressure of the robot movement, as specified by the ISO/TS, can now be measured precisely and therefore validated using PROBms. User software and product training complete the overall package. The worldwide rental concept guarantees that users always have an up-to-date measurement system at their disposal. So PROBms ensures greater productivity and safety on HRC applications.

Press message
The new safety laser scanner PSENscan from Pilz safely monitors up to three separate zones. That increases the productivity of laser-based applications significantly.

Ostfildern, 29Mar.,2017

Safety laser scanner PSENscan from Pilz expands the automation portfolio - in series more productive in 2D

The new safety laser scanner PSENscan from Pilz safely monitors up to three separate zones simultaneously, significantly increasing plant productivity. Up to four safety laser scanners can be connected in series in accordance with the master-slave principle, which reduces the cabling and set-up work considerably. Thanks to the free configuration of warning zones and protection zones plus the ability to adapt to existing structural conditions, PSENscan can easily be integrated into the most varied applications.

Press message
"We are driving change": Safe robotics is one of the future markets for the automation company Pilz

Ostfildern, 29Mar.,2017

For the first time ever, Pilz achieved a turnover of over 300 million Euro and is investing in research and development at its headquarters - "We are driving change"

The Pilz GmbH & Co. KG group of companies continued to grow during the last financial year: The automation company from Ostfildern near Stuttgart increased its turnover to 306 million Euro as well as increasing its number of employees to around 2,200 in 40 subsidiaries. Pilz is currently investing around seven million Euro in its headquarters in Ostfildern to expand research and development. At the end of 2017, Chair of the Board Renate Pilz will leave the operational side of the business and hand the management of the family business completely over to her daughter Susanne Kunschert and son Thomas Pilz.

Press message
From Version 3.0, the speed monitor PNOZ s30 from the safety relay PNOZsigma product group from Pilz has a new analogue output, enabling user-friendly diagnostics.

Ostfildern, 20Mar.,2017

Speed monitor PNOZ s30 from Pilz with a new analogue output - Making safe turns easy

From Version 3.0, the speed monitor PNOZ s30 from the safety relay PNOZsigma product group has a new feature: a configurable analogue output, which makes diagnostics more user-friendly. PNOZ s 30 from Pilz safely monitors standstill, speed, speed range, direction of rotation and broken shear pin up to the highest category PL e/SIL CL 3.

Press message
Under the motto "We automate. Safely." Pilz will be presenting industry solutions, product innovations and services for complete automation solutions at the Hannover Messe from 24 to 28 April 2017.

Ostfildern, 16Mar.,2017

Pilz at COMPONENTS SPECIAL TRADE FAIR BY INTERPACK 2017 in Düsseldorf, Hall 18, Stand B16 - Smart, safe packaging!

At this year's "Components Special Trade Fair by Interpack", the automation company Pilz will be focusing on flexible and economical solutions for packaging machines. The key areas will be solutions around the Smart Factory. Also new in Düsseldorf: the electrically activated E-STOP pushbutton PITestop active, which provides safety and productivity in the spirit of Industrie 4.0, particularly in the packaging sector.

Press message
Start of cooperation on the issue of Industrie 4.0. The Australian Ambassador to Germany, Lynette Wood (centre), and the Australian Consulate-General, Richard Leather (left), spoke to Susanne Kunschert (right) about the route to the industry of the future

Ostfildern, 15Mar.,2017

Australian Ambassador to Germany visits Pilz in Ostfildern - opportunities in automation the focus

On 14.03.2017, the Australian Ambassador to Germany, Lynette Wood, and the Australian Consulate-General, Richard Leather, visited the automation company Pilz in Ostfildern to find out more about the medium-sized enterprise's solutions for the factory of the future. The talks also covered the importance of values in order for Industrie 4.0 to succeed.

Press message
Under the motto "We automate. Safely." Pilz will be presenting industry solutions, product innovations and services for complete automation solutions at the Hannover Messe from 24 to 28 April 2017

Ostfildern, 7Mar.,2017

Pilz at the Hannover Messe 2017, Hall 9, Stand D17 - More intelligent automation!

Under the motto "We automate. Safely." Pilz will be presenting industry solutions, product innovations and services for complete automation solutions at the Hannover Messe from 24 to 28 April 2017. This year's stand focuses on innovative new products for human-robot collaboration (HRC), sensor technology and the intelligent factory.

Press message
With PITestop active, Pilz has a new range of E-STOP pushbuttons that can be activated electrically. It indicates by illumination whether or not it is active. Photo: Pilz GmbH & Co. KG

Ostfildern, 23Feb.,2017

Pilz is presenting a new range of E-STOP pushbuttons PITestop active - Switch smartly – save energy

With PITestop active, Pilz has a new range of E-STOP pushbuttons that can be activated electrically. It indicates by illumination whether or not it is active. So you ensure greater flexibility and modularisation, completely in the spirit of Industrie 4.0. Users also benefit from a reduction in energy costs: that's because it is no longer necessary to keep power applied to the entire plant in order to maintain the E-STOP function.

Press message
The PASloto software from Pilz documents lockout-tagout procedures – the safety-related lockout and interlocking of technical installations. (Photo: Pilz GmbH & Co. KG)

Ostfildern, 20Feb.,2017

PASloto: Manage hazardous energy safely

With PASloto, the automation company Pilz now offers a software package to document lockout-tagout processes (LoTo). As a result, job specifications for dealing with hazardous energy sources can be produced and documented simply. In the associated training course, Pilz also conveys the necessary knowledge about the LoTo procedure and covers the optimum way to work with the software.

Press message

Ostfildern, 21Dec.,2016

New light grids PSENopt slim from Pilz for applications where space is at a premium – protection for the narrowest spaces

Pilz is expanding its range of light beam devices with the PSENopt slim range. With their slimline design, they are suitable particularly in applications where space is at a premium. Here the new super slimline light beam devices provide finger and hand protection, depending on the requirement, up to the highest Performance Level (PL) e.

Press message
With the new generation PSSuniversal 2, Pilz is continuing the success story of the universal remote I/O systems and control systems from Pilz.

Ostfildern, 28Nov.,2016

New generation: Remote I/O system PSSuniversal 2 - Safety and automation right up to the periphery

Pilz is launching a new generation of field level devices with the decentralised I/O system PSSuniversal 2. It consists of the PROFINET communication module and a selection of I/O modules. PSSuniversal 2 provides flexibility, openness and granularity in one system – for safety and automation. The merging of automation and safety functions along with both technical and mechanical improvements help users to save time and costs right from the planning phase.

Press message
Maximum design of the configurable control system PNOZmulti 2: – up to 12 safe expansion modules and a new standard output module are now available for automation.

Ostfildern, 21Nov.,2016

Configurable control systems PNOZmulti 2 for safety and automation with even more connection options - More, faster, greater flexibility

The base unit of the configurable control system PNOZmulti 2 has grown: up to 12 safe expansion modules can now be connected on the right-hand side; a new output module with 14 semiconductor outputs for standard applications is also available. So larger projects can now be implemented simply and flexibly with PNOZmulti 2; several projects can also be managed in parallel.

Press message
With PMCprimo MC, Pilz presents a new external control solution, which can now also be used in more complex plant and machinery thanks to its increased performance.

Ostfildern, 29Sep.,2016

Pilz presents a new stand-alone motion control system - More power to move!

With PMCprimo MC Pilz now offers a new, stand-alone motion control solution. With a 1.3 GHz processor, PMCprimo MC provides the very high performance needed for higher productivity and process quality. Thanks to its increased performance, the scalable motion control solution can now also be used in more complex plant and machinery.

Press message
At SPS IPC Drives 2016 Pilz will be exhibiting automation solutions for the smart factory. The modular production line illustrates how distributed automation systems communicate with sensor and actuator technology.

Ostfildern, 27Sep.,2016

Pilz at SPS IPC Drives 2016: Focus on safe robotics and smart factory - Safe answers for automation

How can genuine human-robot collaboration (HRC) be implemented safely? And how do design engineers and users maintain an overview, particularly with modular and distributed plant and machinery? Visitors to the Pilz stand at SPS IPC Drives 2016 will receive specific answers to these questions. In Nuremberg the automation solution supplier will be exhibiting new products and services for safe robotics and for automation in the smart factory.

Press message
New trainees and dual system students on their first day at Pilz.

Ostfildern, 6Sep.,2016

Start of the new training year at Pilz in Ostfildern – Education without limits

The new training year started at the automation company Pilz in Ostfildern on 5 September. A total of six trainees and 6 students from the dual system offered by the Esslingen University of Applied Sciences (DHBW) are starting their professional careers. In addition to the training places, Pilz also offers a wide range of internships, providing support with career choice orientation. This traditional company is deeply rooted in the region, acting as mentor and providing support as a member of the "Society of Friends of Esslingen University of Applied Sciences".

Press message
Pilz celebrated the opening of its newest subsidiary - Pilz South East Asia - in Singapore. Together with Minister of State Dr. Mohamad Maliki Bin Osman (right), Renate Pilz - Chair of the Board - signed a plaque in commemoration.

Ostfildern, 25Aug.,2016

Reliable automation solutions for Southeast Asia – Pilz opens a subsidiary in Singapore

The automation company Pilz is expanding support to its customers in Southeast Asia: Together with guests from the worlds of politics and business, Pilz celebrated the opening of its newest subsidiary - Pilz South East Asia - in Singapore. From Singapore, customers in the ASEAN region will receive comprehensive support from a dedicated sales and service organisation.

Press message
The automated table football from Pilz combines sensor, control and drive technology.

Ostfildern, 9Aug.,2016

Pilz at Motek 2016 – safe drive solutions for assembly and handling technology – Move it like Pilz!

At this year's Motek, the automation company Pilz will be exhibiting products and solutions for complete automation – from sensor and control technology to drive technology, including operation and visualisation. The stand in Stuttgart will focus on safe drive solutions with safe motion and safe sensor technology PSEN. Visitors to the stand will also be able to obtain comprehensive information about machinery safety and the corresponding range of services, including for drive solutions.

Press message
WindEnergy Hamburg 2016: Pilz offers reliable components and solutions that are already proven in wind energy. Operators benefit from the simple integration of safety systems, remote diagnostic options, remote maintenance and rugged product types.

Ostfildern, 3Aug.,2016

Pilz at WindEnergy Hamburg (27-30 September 2016), Hall B6, Stand B6.342 – Simple, safe automation of wind turbines

At WindEnergy Hamburg Pilz will be exhibiting automation solutions that can be used to monitor safety functions and operating modes on wind turbines. The main focus of the Pilz stand will be on safe speed monitoring, which allows wind turbines to operate efficiently in compliance with the standards. Some of the innovations on display include an I/O module for safe speed monitoring in the automation system PSS 4000. In Hamburg Pilz will also be providing information about its range of services en route to CE marking.

Press message
The automation company Pilz provides industry-proven solutions for monitoring level crossings, safe point setting and protection for passenger transportation.   Photo: vitalytitov/Depositphotos.com

Ostfildern, 19Jul.,2016

Pilz at InnoTrans 2016 in Berlin (20-23 September), Hall 6.2, Stand 405 – Digital control technology for railways: safe and economical

At the InnoTrans 2016 exhibition the automation company Pilz will be showing how industry-proven automation technology can be used in the railway sector. The stand will focus on the automation system PSS 4000-R, which enables Industrie 4.0 mechanisms to be transferred to railway technology. Pilz solutions can be used in applications up to the highest safety integrity level SIL 4; they also meet the normative requirements of CENELEC and support the open RaSTA protocol. Pilz uses virtual reality to help exhibition visitors experience the wide range of application areas for Pilz control solutions.

Press message
The CMSE® Community is a global community of machinery safety experts.

Ostfildern, 31May,2016

Pilz launches international online community for CMSE® - Certified Machinery Safety Experts Strong community for worldwide machinery safety

Since 2013 the automation company Pilz has been working with TÜV Nord to offer the CMSE® - Certified Machinery Safety Expert qualification. More than 1,800 experts in over 40 countries have passed the corresponding examination. Now they can all use www.cmse.com to network, with access to exclusive, practical content.

Press message
The path to safe human-robot-collaboration: On the Automatica 2016 Pilz shows what to take into account during implementation.

Ostfildern, 9May,2016

Pilz on the Automatica 2016 in Munich (21.-24. June), hall B4, stand 500 - With safety man and robot come closer

On the Automatica fair, Pilz puts the focus on the safe human-robot-collaboration (HRC). Based on two model plants, the automation company shows the practicable ways today to safe HRC and it also gives an outlook on future safety technologies. For the first time, Pilz presents its collision measurement device for standard-compliant validation of HRC in accordance with the new ISO/TS 15066.

Press message
The new product range PMI (Pilz Machine Interface) 6 Control from Pilz is equipped with a soft PLC. This terminal goes beyond professional diagnostics and visualisation so that now it is also possible to control the entire plant process.

Ostfildern, 22Apr.,2016

New operating and monitoring product range PMI 6 Control from Pilz - Visualisation and control in one package

With its new product range PMI (Pilz Machine Interface) 6 Control, the automation company Pilz is introducing its first operator terminal to be equipped with a soft PLC in accordance with IEC 61131-3 as standard. This terminal goes beyond professional diagnostics and visualisation, making it possible to control the entire plant process in just one unit. So PMI 6 Control not only offers comprehensive diagnostics but also helps to increase the productivity of the "plant in view".

Press message
Martin Frey (51) is the new Head of Sales Germany in the Automation company Pilz in Ostfildern.

Ostfildern, 21Apr.,2016

Pilz strengthens greater proximity to the customers by expanding its sales network – Martin Frey new Head of sales at Pilz in Germany

Since 1. April 2016 Martin Frey has been the new Head of sales at Pilz. Frey used to work as the head of the Southwest Sales Region at Pilz. He follows Stefan Olding, who left the company of his own accord. Frey wants to expand the sales network of Pilz in Germany, and intensify customer contact together with his sales staff on site.

Press message
Pilz is presenting the light grids PSENopt II at the 2016 Hannover Messe as a world first that enable applications from the category PL d in accordance with EN 61496 as type 3 light grids.

Ostfildern, 6Apr.,2016

New light grids PSENopt II for applications up to PL d - Just the type you need!

The automation company Pilz is presenting a world first for this industry with the first type 3 light grids: As of now, the new light grids PSENopt II enable applications from the category performance level d (PL d). The new light grid type thereby closes the "type gap" of the revised version of IEC 61496-1. With PSENopt II it is no longer necessary to switch to type 4 when PL d is required. The level that precisely matches the safety requirement can now be implemented with the new light grids. This saves costs in the end as overdimensioning is not necessary.

Press message
The family-owned company Pilz posted a new record revenue total of 288 million Euros in 2015. Pilz develops automation solutions for the digital factory. These are also used on its own integrated production line at the headquarters in Ostfildern.

Ostfildern, 6Apr.,2016

Pilz increases revenue, employees and export share in 2015 - "Healthy growth under own momentum"

The group of companies under Pilz GmbH & Co. KG, with its headquarters in Ostfildern near Stuttgart, can look back on the 2015 fiscal year with satisfaction. The family-owned business increased its revenue by 11 percent to 288 million Euros. The employee total also reached a new record level last year: it was up 6 percent at 2,030. With an R&D ratio of 19.8 percent of revenue in 2015, Pilz reaffirms its credentials as one of the most innovative businesses in the field of automation technology.

Press message
The robust safety gate system PSENmlock from Pilz combines safe guard locking with personnel and process protection in one device and is particularly suitable for machines with a hazardous overrun.

Ostfildern, 18Mar.,2016

Pilz introduces a new safety gate system PSENmlock - Reliable door guard

Pilz is adding PSENmlock to its range of safety gate systems with immediate effect. PSENmlock offers safety gate monitoring and safe guard locking for the protection of personnel and processes to the highest category PL e in one device. The slimline yet robust design and the many different installation options make PSENmlock both flexible to use and easy to install.

Press message
Pilz's innovations at the Hannover Messe 2016  include the new diagnostic solution

Ostfildern, 11Mar.,2016

New diagnostic solution: "Safety Device Diagnostics" from Pilz - Reliable diagnostics!

The automation company Pilz is expanding its portfolio to include the diagnostic solution "Safety Device Diagnostics", which comprises a fieldbus module, junction and safe sensor technology PSEN. The new diagnostic solution enables a wide range of sensor data to be called up simply, including over distance. Service operations can be considerably reduced as a result, significantly increasing productivity.

Press message
Under the motto

Ostfildern, 23Feb.,2016

Pilz at the Hannover Messe 2016, Halle 9, Stand D17 - Your way of Automation!

Under the motto "We automate. Safely." Pilz will be presenting industry solutions and services for safety and automation at this year's Hannover Messe from 25 - 29.4.2016. The automation company will also be presenting its product innovations from the fields of "Sensor technology" – including a world first – and "Operating and monitoring".

Press message
Absolute novelty in the failsafe section: The "Non-persistent online change" function can be used to transfer individual changes in the user programs to the control system of the automation system PSS 4000.

Ostfildern, 14Jan.,2016

Release 13 of the automation system PSS 4000 from Pilz enables changes at runtime for safety applications – "Online Change" for safe automation for the first time

The "Non-persistent online change" function" can be used to transfer individual changes in the user programs to the control system. Now Pilz provides this function in the automation system PSS 4000 also for safety applications. Users will save time, because there is no need to compile and load the whole program during commissioning. The function is a component of release 13 of the automation system PSS 4000. Among the further innovations there is a device interface for communication with Profinet networks.

Press message
"Pilz is at the very pulse of development": EU Commissioner Günther H. Oettinger (centre) and Guido Wolf (MdL) (left) visited the automation company Pilz to find out more about the status of Industrie 4.0 among SMEs. Lucas Fischer (right) from Pilz, an electronics student at the Baden-Württemberg Cooperative State University, showed the EU Commissioner how whole plants can be controlled safely using software from Pilz.

Ostfildern, 27Nov.,2015

Information exchange on the subject of Industrie 4.0, between Pilz and EU Commissioner Günther H. Oettinger: "MSEs must take an aggressive approach to digitalisation"

Industrie 4.0 was the focus when Günther H. Oettinger, EU Commissioner for Digital Economy and Society, visited the automation company Pilz in Ostfildern. At Pilz's headquarters he opened the new training workshop, in which professionals for the industry of the future will train for their qualifications. During his visit, EU Commissioner Oettinger also learned about control solutions for the networked factory. Finally, as a manufacturing company Pilz provided some insights into the opportunities and challenges for SMEs in the area of Industrie 4.0. The EU Commissioner was accompanied by Guido Wolf (MdL), the CDU's front runner for the state elections in Baden-Württemberg in 2016, as well as Andreas Deuschle (MdL).

Press message
Safe drive solutions PMC from Pilz can be used flexibly and independently of the higher-level operational control system. PMC is even more open now through the new PROFINET interface for the servo amplifiers PMCprotego D and PMCprotego DD5.

Ostfildern, 23Nov.,2015

Safe Motion from Pilz now also for PROFINET

Safe drive solutions from Pilz Pilz PMC (Pilz Motion Control) now have an interface also for PROFINET. This new communication connection is available for the servo amplifiers PMCprotego D and PMCtendo DD5. With the safety card PMCprotego S, PMCprotego D can be additionally expanded with Safe Motion functions. Safe Motion reduces setup times and maintenance costs and so increases productivity.

Press message
Pilz is adding a new base unit to its range of configurable control systems PNOZmulti 2  PNOZ m B1.

Ostfildern, 23Nov.,2015

New base unit in the configurable control system PNOZmulti 2 from Pilz – Basis for large projects!

Standards for safety, more connections and simpler project management – Pilz is adding its new base unit PNOZ m B1 to the range of configurable control systems PNOZmulti 2. Not only does it offer higher performance for machines with a larger function range, i.e. for larger projects, but it also provides a connection to all common fieldbus systems via the corresponding expansion modules.

Press message
Politics and enterprises in dialogue: The chairman of the FDP Christian Lindner (middle) asked about the activities of the automation company Pilz with the FDP Landtag candidates Stefanie Knecht (second from left) and Erdal Özdogan (second from right). Managing partner Thomas Pilz (right) and Head of Marketing Horst-Dieter Kraus (left) were available to answer questions.

Ostfildern, 13Nov.,2015

Christian Lindner "Politics must strengthen medium-size enterprises" – FDP head Lindner visits Pilz

The automation company Pilz in Ostfildern received a visit from the federal chairman of the FDP, Christian Lindner, on 11. November 2015. The focus of the visit was the open exchange of experiences between the family business and the Liberal Democrats. Christian Lindner was accompanied by the FDP Landtag candidates for Ludwigsburg (Stefanie Knecht) and Esslingen (Erdal Özdogan).

Press message
In building the new Peter Pilz Production and Logistics Centre, Pilz is expanding its headquarters in Ostfildern into the Pilz Campus. Pilz is introducing intelligent production as its contribution to Industrie 4.0.

Ostfildern, 1Oct.,2015

Expansion of headquarters into Pilz Campus – Renate Pilz: “Values create future.” Peter Pilz Production and Logistics Centre opened

The automation company Pilz has opened the Peter Pilz Production and Logistics Centre at its headquarters in Ostfildern. The new building covers a total area of around 13,500 m2 and at EUR 20 million is the largest single investment in the history of this family business. As a result, not only is the company enlarging its production area by 50 per cent, it is also expanding its headquarters into the Pilz Campus.

Press message
Armin Glaser, Vice President Product Management Pilz GmbH & Co. KG

Ostfildern, 1Oct.,2015

Digitisation, internationalism and the role of humans are in the spotlight – the future of automation is safe

It is always expected to be present, but only when it is absent is it actually noticed: safety has the task of protecting people, machinery and the environment. In the past, safety and automation were usually regarded as two separate systems with at least partly conflicting goals. Practice shows that considering the safety functions together with automation technology creates a distinctly better starting position. The challenges of automation can thus be tackled with much greater ease.

Press message
Renate Pilz, Chair of the Board of Pilz GmbH & Co. KG

Ostfildern, 1Oct.,2015

Value orientation for success – values create future

The year 2015 is an especially memorable one for Pilz: - Opening of the first production site outside Europe – in Jintan, China - Construction of new Peter Pilz Production and Logistics Centre in Ostfildern and expansion into Pilz Campus - New logo visually underlines positioning as a supplier of complete solutions for safety and automation. - Pilz brings own web-based visualisation software PASvisu onto the market - The number of employees will exceed 2000 this year for the first time ever. So the signs point to growth at Pilz. Its values and core beliefs are the springboard.

Press message
Dirk Sonder, Senior Vice President Production, Pilz GmbH & Co. KG

Ostfildern, 1Oct.,2015

Pilz creating basis for further growth with new production sites – exemplary manufacturing in the model state

Dirk Sonder, Senior Vice President Production Pilz GmbH & Co. KG In building the new Peter Pilz Production and Logistics Centre, Pilz is not only expanding its production area at its headquarters in Ostfildern: flexible, production-centred hall design, energy efficiency, integrative design of processes and working environment as well as a clear Industrie 4.0 focus are establishing the basis for the further growth of the company.

Press message
Pilz offers manufacturers and operators complete solutions for safety and automation. At SPS IPC Drives 2015 in Nuremberg Pilz will be showing scalable solutions with sensor, control and drive technology, completed by the appropriate operator and visualisation systems.

Ostfildern, 24Sep.,2015

Pilz at SPS IPC Drives (Hall 9, Stand 370) – One-stop safety and automation

At this year's SPS IPC Drives exhibition in Nuremberg (24. - 26.11.2015), Pilz will be showing its range of complete solutions for automation tasks: from sensor technology to control and drive technology – one-stop safety and automation! Pilz will also be exhibiting automation concepts for Industrie 4.0 along with other partners of the research platform SmartFactory KL, on a shared stand in Hall 3a.

Press message
For each cohort of trainees the automation company Pilz, from Ostfildern near Stuttgart, offers not only apprenticeships as “Mechatronics Engineers” and “Electronics Engineers for Equipment and Systems”, but also dual courses of study in partnership with the Baden-Württemberg Cooperative State University

Ostfildern, 14Sep.,2015

As well as apprenticeships, Pilz also offers dual courses of study – the opportunity to start training at Pilz

The new training year has started at Pilz in Ostfildern. A total of five apprentices and nine students of the Baden-Württemberg Cooperative State University (DHBW) are starting their careers at the automation company.

Press message
The new compact I/O module PSSu K F EI with local fast shutdown now enables advanced motion monitoring functions with the control systems PSSuniversal PLC and PSSuniversal multi from the automation system PSS 4000. The new compact module monitors safe speed, direction of movement and stop functions.

Ostfildern, 13Jul.,2015

Pilz completes its solutions portfolio for safe motion monitoring - New module for motion monitoring

Pilz is expanding the performance range of its automation system PSS 4000 for safe motion monitoring: the new, compact I/O module PSSu K F EI monitors safe speed, direction of movement and stop functions. Users benefit from reduced reaction times and higher productivity, as well as simpler maintenance repair of their plant and machinery.

Press message

Stuttgart/Ostfildern, 3Jul.,2015

Staufer Gold Medal for Renate Pilz – Prime Minister Kretschmann: Model family business that creates values by living its values

On 03.07.2015, Renate Pilz, Chair of the Board of Pilz GmbH & Co. KG, was awarded the Staufer Gold Medal. The Prime Minister of Baden-Württemberg Winfried Kretschmann presented the medal at a ceremony in Stuttgart. The Staufer Medal is a special, personal honour awarded by the Prime Minister for services to the State of Baden-Württemberg and its people.

Press message
Pilz supplies Industry 4.0-compatible control systems to plant and machine builders all over the world. Complete

Ostfildern, 25Jun.,2015

Pilz achieves new record values for turnover and number of employees – Strong foundation for cutting edge technology

The Pilz group of companies based in Ostfildern near Stuttgart enjoyed a successful end to the 2014 financial year. The family business increased its turnover to the new record value of 259.3 million Euro. This means an increase of 11.3 per cent over 2013 for the world market leader in safety relays and safety control systems. The number of employees also rose last year: by 6.3 per cent to 1,922.

Press message
With an an official ceremony Pilz opens its first production site in Asia, in the Chinese city of Jintan. From left: Rachel Wang (General Manager of Pilz China), Li Hao (Deputy Mayor of Jintan), Thomas Pilz (Managing Partner of Pilz GmbH & Co. KG), Di Zhi Qiang (Mayor of Jintan), Renate Pilz (Chair of the Board, Pilz GmbH & Co. KG), Shen Xin Feng (Party Secretary of the Administrative Committee of JTDZ), Susanne Kunschert (Managing Partner of Pilz GmbH & Co. KG)

Ostfildern, 17Jun.,2015

Safe automation for Chinese industry – Pilz opens production site in China

The automation company Pilz has opened a production site in the Chinese city of Jintan. In its first production site outside of Europe, the family business from Baden-Württemberg will produce PNOZ safety relays to its company-wide quality standards. As a result, Pilz will be able to supply the growing Chinese market more quickly and consolidate its position there.

Press message
Congratulations: In Sydney, Australia Electrical engineer Rod Burton (right) from Machinery Automation & Robotics, receives the 1000th accreditation of CMSE® - Certified Machinery Safety Expert after successfully passing the end-of-course exam.  Scott Moffat (left), Managing Director of Pilz Australia and New Zealand, presents the certificate.

Ostfildern/Sydney, 20May,2015

CMSE® sets standards for certified, international machinery safety qualification 1,000 CMSE® - Certified Machinery Safety Experts – powered by Pilz

In 2013 Pilz worked with TÜV NORD to develop the international qualification CMSE® - Certified Machinery Safety Expert. This qualification programme teaches extensive knowledge of the machine lifecycle in 22 countries worldwide. In Australia, the 1,000th delegate has now obtained the qualification. That's just one of the reasons why CMSE® has become an international standard for certified training in machinery safety.

Press message
During their tour of the exhibition at the Hannover Messe, Chancellor Angela Merkel (3rd from left) and Narendra Damodardas Modi, Prime Minister of the Republic of India (centre), visited the automation company Pilz. Both were welcomed by Renate Pilz, Chair of the Board (3rd from right), daughter Susanne Kunschert (2nd from right) and son Thomas Pilz (right), both Managing Partners in the family business.

Ostfildern/Hannover, 13Apr.,2015

Renate Pilz: "Safe automation is a success factor for the industry of the future" – Chancellor Merkel visits Pilz at the Hannover Messe

As part of her opening tour of the Hannover Messe 2015, Chancellor Dr. Angela Merkel visited the stand of the automation company Pilz. She was accompanied by Narendra Damodardas Modi, Prime Minister of the Republic of India, this year's partner country of the exhibition. Renate Pilz, Chair of the Board, welcomed the guests and introduced the family business and its global commitment to the safe automation of plant and machinery.

Press message
From April 2015 Pilz will have a new logo. The new logo puts automation firmly back in the spotlight alongside safety as the core competency.

, 10Apr.,2015

Safety and automation: Pilz underlines its positioning – New logo highlights "All in One" in automation

Automation company Pilz renews its brand identity. The family business from Ostfildern is introducing its new logo at the Hannover Messe. The intention of Pilz is to underline visually its positioning as a supplier of complete solutions for safety and automation.

Press message
Pilz is expanding the safety gate system PSENslock to include two new product types: Expanded diagnostic functions are now available, plus the ability to switch OSSD outputs (Output Signal Switching Device) independently from the respective guard locking device.

Ostfildern, 9Apr.,2015

A plus for diagnostics and design freedom

Pilz is expanding the safety gate system PSENslock to include two new product types: one type offers expanded diagnostic functions, while the other type enables OSSD outputs (Output Signal Switching Device) to be switched independently from the guard locking device. So PSENslock can either provide faster diagnostics or greater design freedom, depending on the task.

Press message
Communication modules are now available for the configurable control systems PNOZmulti 2, for connection to Ethernet-based systems.

Ostfildern, 24Feb.,2015

Configurable control systems PNOZmulti 2 for PROFINET and Ethernet/IP

The configurable control system PNOZmulti 2 for safety and automation from Pilz has two new communication modules for connection to Ethernet-based systems. With these, the base unit can now be expanded on the left-hand side and can easily be connected to PROFINET or Ethernet/IP networks. As an open, configurable control system, PNOZmulti 2 can be used flexibly across industry, independently of the higher-level operational control system.

Press message
With its automation system PSS 4000, Pilz is pursuing a consistently mechatronic approach. The modular design of a plant can be mapped in the software platform PAS4000.

Ostfildern, 6Feb.,2015

Pilz is a new member of the research platform SmartFactory KL – Working together for standards with Industry 4.0

Pilz is a new member of the demonstration and research platform SmartFactory KL. As such, the complete safe automation supplier will be actively involved in formulating unified standards for Industry 4.0. The first joint project is to implement a storage module for the smart factory demonstrator at the Hannover Messe 2015.

Press message
The automation system PSS 4000 works in conjunction with safe sensor technology PSEN to guarantee safety in the laser welding laboratory for high-performance laser welding technology at MEYER WERFT.

Ostfildern, 12Nov.,2014

MEYER WERFT uses safety solution from Pilz

MEYER WERFT in Papenburg has equipped its laser welding laboratory for high-performance laser welding technology with a safety solution comprising the automation system PSS 4000, safe sensor technology PSEN and control and signal devices from Pilz. In conjunction with the safety gate system PSENsgate and the operating mode selector switch PITmode, PSS 4000 controls and monitors all the safety functions in the laser welding laboratory, meeting the highest safety requirements up to Performance Level e and Safety Integrity Level 3.

Press message
The new web-based visualisation software from Pilz is based on the latest web technologies and represents a high-performance, easy-to-use solution for operating and monitoring.

Ostfildern, 11Nov.,2014

New web-based visualisation software PASvisu by Pilz - Your automation at a glance

With the web-based visualisation software PASvisu Pilz is launching a high-performance yet simple to use software package for operating and monitoring. The company has developed a platform-independent visualisation package based on the latest web technologies such as HTML 5, CSS3 and JavaScript PASvisu is operated intuitively and provides design freedom for projects: it gives users of Pilz control solutions a complete view of their plant. With PASvisu, Pilz is underlining its claim as a complete safe automation supplier.

Press message
The components of the automation system PSS 4000 from Pilz are now approved as safety components for lift applications by TÜV Austria. As a result, lifts and lifting equipment can now be safeguarded safely and efficiently.

Ostfildern, 12Jun.,2014

Automation system PSS 4000 safeguards lift applications

The components of the automation system PSS 4000 are now approved as safety components for lift applications by TÜV Austria. Lift operators and manufacturers can implement the strict safety regulations and specific requirements that are applicable for these applications using the PSS 4000, in a way that's technically independent, flexible and easy to implement.

Press message
Drives can be monitored safely and efficiently using the new motion monitoring modules for the configurable control system PNOZmulti 2 from Pilz, the complete safe automation supplier.

Ostfildern, 17Apr.,2014

New modules for configurable control systems PNOZmulti 2 – Safe motion monitoring for up to two axes

Pilz is expanding its range of configurable control systems PNOZmulti 2 with new safe motion monitoring modules. The two new modules provide safe monitoring of one or two axes in drives; safety functions can be created and monitored with ease. The modules can be used in any industry, but are a particular advantage in machine tool manufacturing.

Press message
With the new safety relay PNOZ c2 from the product range PNOZcompact from Pilz, standard type 4 light beam devices or sensors with safe switching devices (OSSD outputs) can be monitored quickly and safely.

Ostfildern, 4Apr.,2014

New safety relay PNOZ c2 from Pilz - Fast light beam device monitoring

Pilz is now supplying the safety relay PNOZ c2 from the product range PNOZcompact for safe monitoring of all standard type 4 light beam devices or sensors with safe switching devices (OSSD outputs) in accordance with EN 61496. The short reaction time of no more than 12 milliseconds provides added flexibility as light beam devices can be mounted nearer to the hazardous movement. The new PNOZ c2 can be used in all fields of mechanical engineering and meets the highest safety requirements up to Performance Level (PL) e and Safety Integrity Level Claim Limit (SIL CL) 3. The safety relay brings benefits for the series production of machines in particular.

Press message
In the automation system PSS 4000 from Pilz it is now possible to create safety-related and automation programs for the control systems PSSuniversal PLC using the Editor PAS LD in accordance with EN/IEC 61131-3.

Ostfildern, 27Mar.,2014

Pilz expands its selection of editors in the automation system PSS 4000 – New editor PAS LD for safety and automation functions

Pilz is expanding the range of programming tools in the automation system PSS 4000 with the editor PAS LD (Ladder Diagram). It can be used to create safety-related programs, programs for automation tasks or a combination of the two. Within the Pilz automation system the new editor can be freely combined with the other EN/IEC 61131-3 PLC programming languages, so that even complex automation tasks can be handled simply and consistently.

Press message
The operating mode selector switch PITmode from Pilz is now available with optional pictograms for machine tools.

Ostfildern, 6Mar.,2014

New design for Pilz operating mode selector switch PITmode for machine tools - suitable for international use

The proven operating mode selector switch PITmode from Pilz is now available in a new design, with optional pictograms for machine tools. The use of standard symbols makes it ideal for international use. PITmode provides two functions in one compact unit: safe selection of defined operating modes and access authorisation for the machine.

Press message

Ostfildern, 19Feb.,2014

Prime Minister Kretschmann visits Pilz, the technology leaders – Renate Pilz: "Education is the key to safeguarding the future"

The automation company Pilz in Ostfildern received a visit today from the Prime Minister of Baden-Württemberg Winfried Kretschmann. During his visit he learned about its research and development activities and saw the training facilities set up by this medium-sized enterprise. The Prime Minister singled out the achievements of the family-run business. The Management Team emphasised the importance of an education policy that was both technically sound and ethically oriented.

Press message
Wireless system InduraNET p

Ostfildern, 16Mar.,2007

Reliable wireless communication New wireless system from Pilz, specifically for industrial requirements

Under the name InduraNET p (Industrial Radio Network), Pilz has developed a wireless system that specifically and consistently considers the requirements of an industrial environment. Users benefit from much greater flexibility and are able to implement mobile applications which would be very difficult if not impossible to achieve with a cable-based solution. A special feature of InduraNET p is the innovative antenna system with antenna diversity, which guarantees a constant, high quality wireless connection under all application conditions. Intelligent frequency management also enables coexistence with other wireless systems. In the first expansion phase InduraNET p is available for the decentralised control platform PSSuniversal.

Press message
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
Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de