Compare 0
Video tutorials
Canada | english
You have now of 6 products to compare

SecurityBridge

On the safe side with SecurityBridge!

SecurityBridge protects Pilz control systems from manipulation

With SecurityBridge we offer a product for the area of Industrial Security. The SecurityBridge protects the configurable safe small controllers PNOZmulti 2 and the automation system PSS 4000 from manipulation due to unauthorised access. That way you don't even give espionage and manipulation a chance, but guarantee the safety of your staff and the availability of your machine!

SecurityBridge wins GIT Safety Award 2019

GIT Security Award

The application Firewall SecurityBridge occupied the 3. place in the GIT SECURITY Award. The award was presented on 27. November 2018 a the SPS IPC Drives in Nürnberg. 

The GIT SECURITY AWARD is awarded nationally and internationally. Three innovative products with the most votes were selected from six categories altogether. SecurityBridge was competing in "Category A – Safety and IT-Security in Automation, Cyber-Security". It convinced out customers, partners, market participants and the readers of the magazines GIT SICHERHEIT, GIT SECURITY and messtec drives Automation and it won through against a 14 more finalists.

This is how to use SecurityBridge

SecurityBridge can be connected upstream of the base unit of PNOZmulti or the PLC controller PSSuniversal PLC. It acts as a VPN server, over which a virtual private network (VPN) can be established to one or more client PCs (configuration PC). The connection between PC and device is thus protected. Only suitably authorised users can make changes to a project’s configuration. This prevents unauthorised access to the secured network. The result is that the data transfer between the client PC and SecurityBridge is protected against tapping and manipulation.

The SecurityBridge also controls the process data traffic, and it monitors the integrity of the safety system. Changes in the check sum indicate that there are changes in the projects of PNOZmulti and PSS 4000.

SecurityBridge

Benefits at a glance:

Benefits of SecurityBridge
  • Protection from data manipulation by authentication and authorisation management
  • Increases the availability of the plant because only the necessary data (authorised configuration and process data) are transferred
  • Forwarding or process data with a low latency
  • Detects unpermitted changes to the project by monitoring the check sum (CRC)
  • Prevents unauthorised access because there are downstream devices in a protected network
  • Configuration changes to a project can only be performed by users who have a relevant authorisation

Technical features:

  • Web-based user interface for easy configuration, diagnostics and maintenance
  • Connection to the central authentication system via RADIUS
  • Continuous updates, independently of the control system
  • Integral digital inputs and outputs to activate the VPN tunnel, for example
  • VPN server for building a VPN tunnel for safe transfer of data
  • USB interface for saving and restoring the configuration on a USB memory.
  • LED display for error messages and diagnostics
SecurityBridge

Our product range: Industrial Security

Download

Please wait while data is being loaded

Please wait while data is being loaded

Contact

Pilz Automation Safety Canada L.P.
8-6695 Millcreek Drive
Mississauga, ON, L5N 5R8
Canada

Telephone: +1 905 821 7459
E-Mail: info@pilz.ca

Technical Support

Telephone: +1 888-315-PILZ (315-7459)
E-Mail: info@pilz.ca