Global Site | english

Jan 26, 2018

Safe automation 4.0

A wide range of variants with low volumes. That is the prospect offered by future automation. A wide range of variants calls for a flexible solution such as the automation system PSS 4000.

The automation system PSS 4000 is a safe and different approach to automation: specially developed for the requirements of future automation, the system is suitable for flexible and modular use.

With the automation system PSS 4000 you can network multiple PLC controllers in accordance with the Multi-Master principle, yet each one runs autonomously. Each control and I/O component automatically provides process data to all other controllers in the project – without a detour through a centralised control instance.

Your programming is independent from the hardware and you can decide later whether a function is to run in various controllers or just in one controller. Complex programming of the individual communication connections between several controllers is not required. This saves time and prevents errors during programming.

The visualisation software PASvisu further simplifies the engineering process. All data from the automation project can be directly used in the visualisation. Duplicate inputs and resulting error sources are excluded.

The optimum solution for modular and flexible plants in accordance with the Industrie 4.0 benchmark.

 

Further information:

Automation system PSS 4000 distributability
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
  • Belgium: +32 9 321 75 75