Global Site | english

Ostfildern, Apr 17, 2014

New modules for configurable control systems PNOZmulti 2 – Safe motion monitoring for up to two axes

Pilz is expanding its range of configurable control systems PNOZmulti 2 with new safe motion monitoring modules. The two new modules provide safe monitoring of one or two axes in drives; safety functions can be created and monitored with ease. The modules can be used in any industry, but are a particular advantage in machine tool manufacturing.

 

Pilz is expanding its range of configurable control systems PNOZmulti 2 with new safe motion monitoring modules. The two new modules provide safe monitoring of one or two axes in drives; safety functions can be created and monitored with ease. The modules can be used in any industry, but are a particular advantage in machine tool manufacturing.

All safety functions are easy to implement in accordance with EN 61800-5-2 for adjustable speed electrical power drive systems. As such you can achieve optimum availability of plant and machinery, coupled with a high level of safety. All common incremental encoders can also be connected using drive-specific connection cables via the industry-compatible interface Mini I/O.

Extensive motion monitoring functions
Functions include "Safe Speed Range", "Safe Speed Monitoring" or "Safe Direction". "Safe Operating Stop" completes the function range of the motion monitoring modules that form part of the configurable control system PNOZmulti 2. So safe monitoring of drives ultimately results in high plant availability.

Simple handling through configuration software
The new motion monitoring modules for PNOZmulti 2 are configured via the software tool PNOZmulti Configurator. With this tool, users can create and monitor safety functions intuitively, independent of the higher level control system. Instead of carrying out the wiring manually, the safety program can easily be customised for safety-related functions using the certified function blocks stored in the software tool PNOZmulti Configurator. This saves time and money at the planning stage and during configuration, diagnostics and maintenance.

Further information on the product at: https://www.pilz.com/de-DE/eshop/00010000247108/PNOZmulti-2-E-A-Module

Exhibition "Components for processing and packaging", Düsseldorf: Pilz is exhibiting in Hall: CS418.

 

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de