Global Site | english

Ostfildern, Jul 13, 2015

Pilz completes its solutions portfolio for safe motion monitoring - New module for motion monitoring

Pilz is expanding the performance range of its automation system PSS 4000 for safe motion monitoring: the new, compact I/O module PSSu K F EI monitors safe speed, direction of movement and stop functions. Users benefit from reduced reaction times and higher productivity, as well as simpler maintenance repair of their plant and machinery.

Pilz is expanding the performance range of its automation system PSS 4000 for safe motion monitoring: the new, compact I/O module PSSu K F EI monitors safe speed, direction of movement and stop functions. Users benefit from reduced reaction times and higher productivity, as well as simpler maintenance repair of their plant and machinery.

High productivity in manufacturing is closely linked with safe speed and motion monitoring. Pilz now has a new I/O module for the control systems PSSuniversal PLC and PSSuniversal multi from the automation system PSS 4000, designed for safe motion monitoring of machines and distributed plants.

Safe motion monitoring with one rotary encoder
It enables safety functions for speed monitoring in accordance with EN 61800-5-2 with only one Sin/Cosrotary encoder, or in a combination of rotary encoder and proximity switch with additional gear monitoring. The use of just one rotary encoder minimises the installation work. As the module can be connected to all common rotary encoder/feedback systems (sin/cos, TTL, HTL, proximity switches), existing encoder systems can continue to be used.
The new module has local fast shutdown of drives, irrespective of the PLC cycle time. As a result, the reaction time is reduced and plant productivity increased. Up to 8 axes per controller can be monitored up to Performance Level (PL) d. As a result, the motion monitoring solution with PSS 4000 is particularly suitable for larger applications.

Ease of handling
The safe monitoring function is fully integrated within the user software. As a result, users can set up the speed functions via the software tool. Projects can be implemented quickly and can be easily adapted. It is even possible to change threshold values during operation, for example.

With the new encoder module and corresponding software blocks it is possible to implement the safety functions SSM "Safe Speed Monitoring", SSR "Safe Speed Range", SDI "Safe Direction" and SOS "Safe Operating Stop". 

Contact in the subsidiaries:

Australia:
Don Gherashe
Telephone: +61 3 95446300
E-Mail: safety@pilz.com.au

Great Britain:
Natasha Sephton-Pike
Telephone: +44 1536 460766
E-Mail: marketing@pilz.co.uk

India:
Shivani Handoo
Telephone: +91 20 24213994/95
E-Mail: s.handoo@pilz.in

Ireland:
Yvonne McNamara
Telephone: +353 21 4346535
E-Mail: y.mcnamara@pilz.ie

USA and Canada:
Felicia Caponi
Telephone: +1 734 354-0211
E-Mail: f.caponi@pilzusa.com


Contact for the Pilz Group:

Martin Kurth
Corporate and Technical Press
Germany
Telephone: +49 711 3409-158
E-Mail: m.kurth@pilz.de

Sabine Karrer
Technical Press
Germany
Telephone: +49 711 3409-7009
E-Mail: s.skaletz-karrer@pilz.de

The new compact I/O module PSSu K F EI with local fast shutdown now enables advanced motion monitoring functions with the control systems PSSuniversal PLC and PSSuniversal multi from the automation system PSS 4000. The new compact module monitors safe speed, direction of movement and stop functions.
Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de