Global Site | english

Ostfildern, Nov 23, 2015

New base unit in the configurable control system PNOZmulti 2 from Pilz – Basis for large projects!

Standards for safety, more connections and simpler project management – Pilz is adding its new base unit PNOZ m B1 to the range of configurable control systems PNOZmulti 2. Not only does it offer higher performance for machines with a larger function range, i.e. for larger projects, but it also provides a connection to all common fieldbus systems via the corresponding expansion modules.

For the first time, the new base unit PNOZ m B1 contains no inputs or outputs: expansion modules are used to adapt the system to the application. Two integrated Ethernet interfaces save costs, as there is no need to connect an ETH expansion module. The number of expansion modules that can be connected on the right-hand side has been increased to eight on the new base unit. Short downtimes and high plant availability are guaranteed by connection to common fieldbus systems via the respective expansion modules.

Project management made simple
The maximum program size of the PNOZ m B1 has been quadrupled: up to 1024 connections can now be inserted between the elements. Projects can be stored on a USB memory stick. The pluggable USB data medium allows several projects to be stored and enables machine-specific management. One of the programs can be selected to run via the Project Manager. It is also now possible to set the date and time for PNOZ m B1 in the PNOZmulti Configurator. And an illuminated display helps to provide convenient on-site diagnostics. PNOZ m B1 can be used from Version 10 of the software tool PNOZmulti Configurator.

Field connection guaranteed
The configurable control system PNOZmulti 2 can now also be connected to the fieldbus system CC-Link, in addition to Profinet, Profibus, Ethernet/IP and many more. If PNOZmulti 2 is to be connected to another fieldbus system, this can be achieved without having to change the program: that's because one fieldbus module can simply be swapped for another suitable module.

Open for safety
PNOZmulti 2 is an open, configurable control system for safety functions, which can be used flexibly and industry-wide for safety and automation, independently of the higher-level plant control system. Use of the available expansion modules allows finer granularity, enabling the control structure to be adapted precisely to the application. Users only purchase what they will actually use, saving time and costs.

Setting safety standards
The configurable control systems PNOZmulti 2 are particularly suitable for implementing multiple safety functions on plant or machinery. The system is modular and expandable, so it can grow with the machine as it expands or as its requirements change. PNOZmulti 2 can be connected to common communication networks. The safety architecture can be created independently of the higher-level operational control system, because its application is independent of the machine or plant type, country or industry. That's how users standardise their safety.
 

Pilz is adding a new base unit to its range of configurable control systems PNOZmulti 2  PNOZ m B1.
Pilz is adding a new base unit to its range of configurable control systems PNOZmulti 2 PNOZ m B1.

Pilz is adding a new base unit to its range of configurable control systems PNOZmulti 2 PNOZ m B1.

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de