Global Site | english

Ostfildern, Nov 23, 2015

Safe Motion from Pilz now also for PROFINET

Safe drive solutions from Pilz Pilz PMC (Pilz Motion Control) now have an interface also for PROFINET. This new communication connection is available for the servo amplifiers PMCprotego D and PMCtendo DD5. With the safety card PMCprotego S, PMCprotego D can be additionally expanded with Safe Motion functions. Safe Motion reduces setup times and maintenance costs and so increases productivity.

PMCprotego D and PMCtendo DD5 can be used alongside PROFINET in all common fieldbus systems. The interface card is simply plugged into the servo amplifier for almost all relevant fieldbus systems. Thus, the user can save investment costs with the interface for PROFINET network. Pilz servo drive technology is open for individual solutions, the servo amplifiers can practically be integrated in each automation environment.

Pilz also provides support from the safe drive configuration through to commissioning with a comprehensive range of services also for PMC.

Safe drive solutions PMC from Pilz can be used flexibly and independently of the higher-level operational control system. PMC is even more open now through the new PROFINET interface for the servo amplifiers PMCprotego D and PMCprotego DD5.
Safe drive solutions PMC from Pilz can be used flexibly and independently of the higher-level operational control system. PMC is even more open now through the new PROFINET interface for the servo amplifiers PMCprotego D and PMCprotego DD5.

Safe drive solutions PMC from Pilz can be used flexibly and independently of the higher-level operational control system. PMC is even more open now through the new PROFINET interface for the servo amplifiers PMCprotego D and PMCprotego DD5.

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de