Global Site | english

Ostfildern, May 23, 2019

World's first safe radar system solution new to the Pilz portfolio - Safe even in the most rugged environments!

New to the Pilz portfolio is the world's first safe complete solution for protection zone monitoring, based on radar technology. It comprises the safe radar system "LBK System" from Inxpect S.p.A. and the configurable small controller PNOZmulti 2. This complete solution provides safe, economical monitoring even in the must rugged environments – in extreme production environments such as dust in woodworking for example – or with complex plant structures. Benefits of the safe radar system solution include high plant or machine productivity, despite the most rugged environment.

The safe radar system solution expands the Pilz portfolio in the safe sensor technology range PSEN.

System solution comprising radar sensor and controller
The safe radar system solution comprises up to six radar sensors and one control unit, depending on the application. Add to that the configurable safe small controller PNOZmulti 2, which is responsible for safety in the solution. In the event of a fault and when the protection zone is violated, PNOZmulti ensures that the reaction that is triggered is safe and reliable. The safe radar system solution can be used up to SIL 2, PL d, Category 2.
The safety-related functions covered by the system solution include the "detection function", i.e. when a machine is switched to a safe state as soon as a danger zone is violated, plus the restart interlock, which prevents the machine starting automatically if there is anyone in the danger zone. The layout for a protection zone is maximum 15 m x 4 m with an opening angle of 110° horizontal and 30° vertical.

Flexibility for outdoors and other extremes
The layout of the protection zone and system at the site where the safe radar system solution is used can be flexible. The protection zone can be set up as wide or narrow, depending on the size of the area to be monitored. A wide protection zone covers a horizontal opening angle of 110° and a vertical opening angle of 30°. A narrow protection zone has an opening angle of 50° horizontal and 15° vertical. The actual protection zone of the sensor depends on the height at which the sensor is installed and the inclination (horizontal/vertical) of the sensor. A maximum depth of four metres can be set. The system solution can even develop a variety of protection zones via the number and inclination of the sensors, e.g. to form a circular arrangement.

In series for larger applications
The overall area of the application can be increased if six sensors are connected in series and arranged at a maximum distance of 2.5 m apart. This allows up to 15 m to be monitored with a complete solution. Integrated muting not only provides a high level of flexibility but also greater productivity. It can be used either for the overall system solution or for individual sensors.
The corresponding configurator enables you to select the sensors and their configuration. An additional warning zone can be configured here as an option. This saves time, plus the machine can be put into service more quickly.

No problem with dust and dirt
The safe radar technology on which the system solution is based is fundamentally insensitive to external influences such as dust, rain, light, sparks or even shock. So the safe radar system solution can be used anywhere that optoelectronic sensors and technologies cannot guarantee availability. In addition to safe area monitoring with the safe laser scanner PSENscan or the light curtains PSENopt, the world's first safe radar system solution also provides a productive solution in extremely rugged environments – for outdoor use, in heavy industry or woodworking for example.
Typical applications can be found in heavy industry, where dirt, dust, swarf or welding sparks, bright light and shock are prevalent. This includes steel processing, foundries or woodworking. Outdoors, the radar system solution safeguards cranes and floor conveyor systems, bulk cargo ports or storage facilities even in fog, snow and up to moderate rain.

Further information is available here

The world's first safe radar system solution expands the safe sensor technology range PSEN from Pilz.
The world's first safe radar system solution expands the safe sensor technology range PSEN from Pilz.

The world's first safe radar system solution expands the safe sensor technology range PSEN from Pilz.

Headoffice

Pilz GmbH & Co. KG
Felix-Wankel-Straße 2
73760 Ostfildern
Germany

Telephone: +49 711 3409-0
E-Mail: pilz.gmbh@pilz.de

Corporate and Technical Press

Telephone: +49 711 3409 - 158
E-Mail: m.kurth@pilz.de