Global Site | english

Sensor technology

Light beam devices PSENopt

Are body protection light grids available for the PSENopt Advance light grid?

Unfortunately not, but the PSEN op2/4B-x-xx/1 types can be used as an alternative.

Which light grids can be configured with the PSENopt Configurator? The Configurator can be used to configure Type 4 light grids from the PSENopt Advance series.