Global Site | english

Controllers

PLC controllers and I/O systems

How can the control head be reset to the factory default settings?

Original reset: carry out the following steps <10 s

  • Switch off voltage to PSS
  • Remove SD card
  • Switch on voltage to PSS
  • Press reset button >5s until DIAG-LED flashes
  • Release reset button
  • Press reset button
  • Release reset button

The control head will now have the following default settings:

  • Device name: PSS__
  • IP address: 169.254.1.0 to 169.254.254.255 (Auto-IP mechanism)
  • Subnet mask: 255.255.0.0
    SD card can be formatted via a PC.