Global Site | english

Small controllers

Configurable compact controllers PNOZmulti Mini

What are configurable inputs/outputs on the base units from the small controller PNOZmulti Mini?

The PNOZmulti Mini base units have 20 safe inputs, up to 8 of which can be configured as outputs for standard applications. In addition to 4 safe semiconductor outputs there are also 4 semiconductor outputs, which can be configured as outputs for standard applications or as test pulse outputs.

The required function for each of these configurable inputs/outputs can be assigned in the PNOZmulti Configurator. For example, the standard outputs are suitable for messages to higher level controllers.