Global Site | english

Small controllers

Configurable control systems PNOZmulti 2

What are configurable inputs/outputs on the base unit PNOZ m B0 from the PNOZmulti 2?

The PNOZmulti 2 base unit PNOZ m B0 has 20 safe inputs, up to 8 of which can be configured as outputs for standard applications. In addition to 4 safe semiconductor outputs there are also 4 semiconductor outputs, which can be configured as outputs for standard applications or as test pulse outputs.

The required function for each of these configurable inputs/outputs can be assigned in the PNOZmulti Configurator. For example, the standard outputs are suitable for messages to higher level controllers.