Global Site | english

Small controllers

Software small controllers

How can I read and save the error stack?

  1. Call up the error stack in the PNOZmulti Configurator; an online connection is needed.
  2. Using the right mouse button in the error text field, select all under the "Display" menu
  3. Then, under "Save", define the path and file name, ...
  4. ... save and email it to Technical Support (techsupport@pilz.de).
    The file *.mperr can be displayed using any text editor (e.g. Windows text editor).