Global Site | english

Sensor technology

Safety laser scanner PSENscan

How do you switch between the zone configurations?

Up to 3 digital inputs can currently be used for switching. To prevent shorts across contacts, etc., only one input must be on 1 at a time. As a result, there are up to 3 switchable configurations. With the maximum number of zone configurations, no reset/restart and no warning output can be used.

In later versions, up to 70 switchable configurations will be supported.