Global Site | english

CE marking

New CE certification when a machine is relocated from Slovakia to Bulgaria?

Question:

If we take a machine that has been certified in accordance with the Machinery Directive 98/37/EC and relocate it from Slovakia to Bulgaria and then set it back up in exactly the same state, would we need to recertify the machine in accordance with the Machinery Directive 2006/42/EC?

Answer:

As the machine is certified in accordance with the Machinery Directive 98/37/EC, it will not need to be recertified in accordance with the Machinery Directive 2006/42/EC.