Global Site | english

PNOZmulti Configurator Videos

The PNOZmulti Configurator software tool provides support during the project design, configuration, documentation and commissioning of the configurable safe small controllers PNOZmulti. Why not see for yourself! The video tutorials illustrate the most important functions of the PNOZmulti Configurator. For the latest software version you'll find a What’s New Video, which summarises the most important new features.

The video tutorials illustrate the most important functions of the PNOZmulti Configurator

What’s New Video PNOZmulti Configurator

The What’s New Video provides a brief overview of the features on the latest software version of the PNOZmulti Configurator. That way you are always up-to-date on the latest release of the software.

Download the latest version of the PNOZmulti Configurator now

PNOZmulti Configurator Version 10.9 – now also with offline simulation

From Version 10.9 you have the option to test your configured user program prior to commissioning using the "Simulation" function. In a first release you calculate the logic elements, in further releases you calculate all the elements with the simulation. Elements that are not simulated can be switched to the required state by forcing the outputs. This way, you can implement a simulation of the overall application. The targeted forcing of link elements enables you to simulate your application only in parts. This saves you from having to define all the inputs!

PNOZmulti Configurator 10.8

Version 10.8 of PNOZmulti Configurator supports a new expansion module of the configurable small control systems PNOZmulti 2: The safe analogue input module PNOZ m EF 4AI. The expansion module provides four independent safe analogue current inputs. The configuration is mode in the module program mIQ.

You can configure the following monitoring functions in the software tool:

  • Working area monitoring in accordance with the NAMUR NE43 recommendation or freely configurable
  • Scaling function
  • Plausibility check
  • Mathematical operations
  • Constant
  • Threshold value monitoring
  • Range monitoring

For diagnostic purposes, an exact analogue value can be forwarded to a fieldbus or an OPC server. The dynamic program display has been expanded for the analogue modules. The analogue values can also be displayed in a variable list. Find out more from the video about the various functions!